This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

facing problem with zygote service after porting android on dm 365

Other Parts Discussed in Thread: PCA9543A, THS7303, TVP5146, TVP7002, THS7353

HI ALL,

Can any one guide me for the issue i am facing after porting Android(2.3--Ginger Bread) on DM365evm.

i am using linux kernel 2.6.32_rc1,

The main issue is with zygote, please find the output of logcat command:

# init: untracked pid 1729 exited
init: untracked pid 1750 exited

# logcat

I/DEBUG   ( 1726): debuggerd: Dec 28 2011 12:16:22
I/Netd    ( 1725): Netd 1.0 starting
I/Vold    ( 1724): Vold 2.1 (the revenge) firing up
D/Vold    ( 1724): USB mass storage support is not enabled in the kernel
D/Vold    ( 1724): usb_configuration switch is not enabled in the kernel
D/Vold    ( 1724): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
D/AndroidRuntime( 1728):
D/AndroidRuntime( 1728): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 1728): CheckJNI is ON
W/dalvikvm( 1728): JNI_CreateJavaVM failed
E/AndroidRuntime( 1728): JNI_CreateJavaVM failed
I/        ( 1750): ServiceManager: 0xad50
W/AudioHardwareInterface( 1750): Using stubbed audio hardware. No sound will be produced.
D/AudioHardwareInterface( 1750): setMode(NORMAL)
I/CameraService( 1750): CameraService started (pid=1750)
I/AudioFlinger( 1750): AudioFlinger's thread 0xc630 ready to run
D/AndroidRuntime( 1751):
D/AndroidRuntime( 1751): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 1751): CheckJNI is ON
W/dalvikvm( 1751): JNI_CreateJavaVM failed
E/AndroidRuntime( 1751): JNI_CreateJavaVM failed
I/ServiceManager( 1723): service 'media.audio_flinger' died
I/ServiceManager( 1723): service 'media.audio_policy' died
I/ServiceManager( 1723): service 'media.player' died
I/ServiceManager( 1723): service 'media.camera' died

Thanks and regards

Ranjan.D


  • Hi Ranjan,

    Please attach complete bootlog and logcat output to debug this further.

    Regards,

    Pankaj Bharadiya

  • Hi Pankaj,

    I need some clarifications regarding the procedure i am fallowing, kindly help me with that.

    I am using linux kernel 2.6.32_rc1 and enabled android drivers in staging--->android (make menu config) and built it, and by following some of the post  i got the android (ginger bread  2.3) rfs for dm365evm.

    here my question is other than ebabling these staging drivers, are there any patchs to de done for the refrence kernel which i am using (i.e linux kernel 2.6.32_rc1 )? if yes what are those ? 

    From one of the blog i found out  that  Ginger Bread  needs  Linux kernel 2.6.35 or later, and in this case i need support of  RFC for Media Controller capture driver for DM365 and as well as the android sepcific patchs (if applicable) for linux kernel 2.6.35.

    And you can find the detailed logcat output in my next post.

    Thanks and Regards

    Ranjan

  • Hi pankaj,

    You can find the  boot log and logcat command here:

    Filename 'uImage'.
    Load address: 0x80700000
    Loading: *#################################################################
         #################################################################
         ##################
    done
    Bytes transferred = 2165116 (21097c hex)
    DM365 EVM :>setenv rootpath /home/saravana/Rohit/TI_Android_GingerBread_2_3_Sources/out/target/product/dm365evm/Android_rfs
    DM365 EVM :>setenv nfshost 192.168.2.62  54
    DM365 EVM :>setenv bootargs mem=71M console=ttyS0,115200n8 androidboot.console=ttyS0 root=/dev/nfs rw nfsroot=$(nfshost):$(rootpath),nolock ip=dhcp init=/init video=davincifb:vid0=OFF:vid1=OFF:osd0=720x720x16,2025K dm365_imp.oper_mode=0
    DM365 EVM :>bootm 80700000
    ## Booting kernel from Legacy Image at 80700000 ...
       Image Name:   Linux-2.6.32-rc2-davinci1
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2165052 Bytes =  2.1 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux............................................................................................................................................. done, booting the kernel.
    Linux version 2.6.32-rc2-davinci1 (saravana@saravana-Inspiron-580s) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #2 PREEMPT Fri Dec 30 11:55:56 IST 2011
    CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
    CPU: VIVT data cache, VIVT instruction cache
    Machine: DaVinci DM365 EVM
    Memory policy: ECC disabled, Data cache writeback
    DaVinci dm365_rev1.2 variant 0x8
    Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 18034
    Kernel command line: mem=71M console=ttyS0,115200n8 androidboot.console=ttyS0 root=/dev/nfs rw nfsroot=192.168.2.54:/home/saravana/Rohit/TI_Android_GingerBread_2_3_Sources/out/target/product/dm365evm/Android_rfs,nolock ip=dhcp init=/init video=davincifb:vid0=OFF:vid1=OFF:osd0=720x720x16,2025K dm365_imp.oper_mode=0
    Unknown boot option `androidboot.console=ttyS0': ignoring
    PID hash table entries: 512 (order: -1, 2048 bytes)
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 71MB = 71MB total
    Memory: 66880KB available (4056K code, 781K data, 144K init, 0K highmem)
    SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    Hierarchical RCU implementation.
    NR_IRQS:245
    Console: colour dummy device 80x30
    ram_console: buffer (null), invalid size 0, datasize 4294967284
    Calibrating delay loop... 147.86 BogoMIPS (lpj=739328)
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    DaVinci: 8 gpio irqs
    NET: Registered protocol family 16
    davinci_serial_init:97: failed to get UART2 clock
    EVM: HD imager video input
    bio: create slab <bio-0> at 0
    DM365 IPIPE initialized in Continuous mode
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    pca9543a_probe
    vpss vpss: dm365_vpss vpss probed
    vpss vpss: dm365_vpss vpss probe success
    dm365_afew_hw_init
    ch0 default output "COMPOSITE", mode "NTSC"
    VPBE Encoder Initialized
    cfg80211: Using static regulatory domain info
    cfg80211: Regulatory domain: US
        (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
        (2402000 KHz - 2472000 KHz @ 40000 KHz), (600 mBi, 2700 mBm)
        (5170000 KHz - 5190000 KHz @ 40000 KHz), (600 mBi, 2300 mBm)
        (5190000 KHz - 5210000 KHz @ 40000 KHz), (600 mBi, 2300 mBm)
        (5210000 KHz - 5230000 KHz @ 40000 KHz), (600 mBi, 2300 mBm)
        (5230000 KHz - 5330000 KHz @ 40000 KHz), (600 mBi, 2300 mBm)
        (5735000 KHz - 5835000 KHz @ 40000 KHz), (600 mBi, 3000 mBm)
    cfg80211: Calling CRDA for country: US
    LogicPD encoder initialized
    Switching to clocksource timer0_1
    musb_hdrc: version 6.0, cppi-dma, host, debug=0
    musb_hdrc: USB Host mode controller at fec64000 using DMA, IRQ 12
    musb_hdrc musb_hdrc: MUSB HDRC host driver
    musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
    usb usb1: configuration #1 chosen from 1 choice
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    NET: Registered protocol family 2
    IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    TCP established hash table entries: 4096 (order: 3, 32768 bytes)
    TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP reno registered
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    msgmni has been set to 130
    alg: No test for stdrng (krng)
    io scheduler noop registered
    io scheduler anticipatory registered (default)
    davincifb davincifb.0: dm_osd0_fb: Initial window configuration is invalid.
    Console: switching to colour frame buffer device 90x45
    davincifb davincifb.0: dm_osd0_fb: 720x720x16@0,0 with framebuffer size 2025KB
    davincifb davincifb.0: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 1020KB
    davincifb davincifb.0: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB
    davincifb davincifb.0: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 1020KB
    DM365 IPIPEIF probed
    imp serializer initialized
    davinci_previewer initialized
    davinci_resizer initialized
    Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled
    serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
    console [ttyS0] enabled
    brd: module loaded
    at24 1-0050: 32768 byte 24c256 EEPROM (writable)
    Read MAC addr from EEPROM: 00:0e:99:02:cf:80
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
    2 NAND chips detected
    Bad block table not found for chip 1
    Bad block table not found for chip 1
    Scanning device for bad blocks
    Bad eraseblock 8281 at 0x000040b20000
    Bad eraseblock 11595 at 0x00005a960000
    Bad eraseblock 12813 at 0x0000641a0000
    Bad eraseblock 13871 at 0x00006c5e0000
    Bad eraseblock 13909 at 0x00006caa0000
    Bad eraseblock 13931 at 0x00006cd60000
    Bad eraseblock 13953 at 0x00006d020000
    Bad eraseblock 13961 at 0x00006d120000
    Bad eraseblock 13997 at 0x00006d5a0000
    Bad eraseblock 14047 at 0x00006dbe0000
    Bad eraseblock 14083 at 0x00006e060000
    Bad eraseblock 14113 at 0x00006e420000
    Bad eraseblock 14169 at 0x00006eb20000
    Bad eraseblock 14183 at 0x00006ece0000
    Bad eraseblock 14199 at 0x00006eee0000
    Bad eraseblock 14205 at 0x00006efa0000
    Bad eraseblock 14213 at 0x00006f0a0000
    Bad eraseblock 14337 at 0x000070020000
    Bad eraseblock 14339 at 0x000070060000
    Bad eraseblock 14341 at 0x0000700a0000
    Bad eraseblock 14343 at 0x0000700e0000
    Bad eraseblock 14345 at 0x000070120000
    Bad eraseblock 14347 at 0x000070160000
    Bad eraseblock 14353 at 0x000070220000
    Bad eraseblock 14355 at 0x000070260000
    Bad eraseblock 14357 at 0x0000702a0000
    Bad eraseblock 14359 at 0x0000702e0000
    Bad eraseblock 14361 at 0x000070320000
    Bad eraseblock 14363 at 0x000070360000
    Bad eraseblock 14365 at 0x0000703a0000
    Bad eraseblock 14367 at 0x0000703e0000
    Bad eraseblock 14369 at 0x000070420000
    Bad eraseblock 14371 at 0x000070460000
    Bad eraseblock 15663 at 0x00007a5e0000
    Creating 5 MTD partitions on "davinci_nand.0":
    0x000000000000-0x000000f00000 : "bootloader"
    0x000000f00000-0x000001000000 : "params"
    0x000001000000-0x000001400000 : "kernel"
    0x000001400000-0x000021400000 : "filesystem1"
    0x000021400000-0x000080000000 : "filesystem2"
    davinci_nand davinci_nand.0: controller rev. 2.3
    spi_davinci spi_davinci.0: DaVinci SPI driver in EDMA mode
    Using RX channel = 17 , TX channel = 16 and event queue = 3
    at25 spi0.0: 8 KByte at25640 eeprom, pagesize 32
    spi_davinci spi_davinci.0: Controller at 0xfec66000
    console [netcon0] enabled
    netconsole: network logging started
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    usbcore: registered new interface driver usbtest
    mice: PS/2 mouse device common for all mice
    input: DM365 EVM Controls as /devices/platform/i2c_davinci.1/i2c-1/1-0025/input/input0
    i2c /dev entries driver
    Linux video capture interface: v2.00
    ths7303 1-002c: chip found @ 0x58 (DaVinci I2C adapter)
    vpfe_init
    vpfe-capture: vpss clock vpss_master enabled
    vpfe-capture vpfe-capture: v4l2 device registered
    vpfe-capture vpfe-capture: video device registered
    EVM: switch to tvp5146 SD video input
    tvp514x 1-005d: tvp514x 1-005d decoder driver registered !!
    vpfe-capture vpfe-capture: v4l2 sub device tvp5146 registered
    EVM: switch to tvp7002 HD video input
    tvp7002 1-005c: tvp7002 1-005c decoder driver registered !!
    vpfe-capture vpfe-capture: v4l2 sub device tvp7002 registered
    EVM: switch to tvp7002 HD video input
    ths7353 1-002e: chip found @ 0x5c (DaVinci I2C adapter)
    ths7353 1-002e: No platform data!!
    vpfe-capture vpfe-capture: v4l2 sub device ths7353 registered
    vpfe_register_ccdc_device: DM365 ISIF
    DM365 ISIF is registered with vpfe.
    af major#: 252, minor# 0
    AF Driver initialized
    aew major#: 251, minor# 0
    AEW Driver initialized
    Trying to register davinci display video device.
    layer=c3181a00,layer->video_dev=c3181b70
    Trying to register davinci display video device.
    layer=c3181800,layer->video_dev=c3181970
    davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
    watchdog watchdog: heartbeat 60 sec
    davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
    usbcore: registered new interface driver usbhid
    usbhid: v2.6:USB HID core driver
    logger: created 64K log 'log_main'
    logger: created 256K log 'log_events'
    logger: created 64K log 'log_radio'
    Advanced Linux Sound Architecture Driver Version 1.0.21.
    No device for DAI tlv320aic3x
    No device for DAI davinci-i2s
    asoc: tlv320aic3x <-> davinci-i2s mapping ok
    ALSA device list:
      #0: DaVinci EVM (tlv320aic3x)
    TCP cubic registered
    NET: Registered protocol family 17
    lib80211: common routines for IEEE802.11 drivers
    Clocks: disable unused mmcsd1
    Clocks: disable unused spi1
    Clocks: disable unused spi2
    Clocks: disable unused spi3
    Clocks: disable unused spi4
    Clocks: disable unused pwm0
    Clocks: disable unused pwm1
    Clocks: disable unused pwm2
    Clocks: disable unused pwm3
    Clocks: disable unused timer1
    Clocks: disable unused timer3
    Clocks: disable unused emac
    Clocks: disable unused voice_codec
    Clocks: disable unused rto
    Clocks: disable unused mjcp
    emac-mii: probed
    eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, id=221613)
    Sending DHCP requests .
    PHY: 1:01 - Link is Up - 100/Full
    ., OK
    IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.2.220
    IP-Config: Complete:
         device=eth0, addr=192.168.2.220, mask=255.255.255.0, gw=192.168.2.1,
         host=192.168.2.220, domain=fossilshale.org, nis-domain=(none),
         bootserver=0.0.0.0, rootserver=192.168.2.54, rootpath=, mtu=1500
    Looking up port of RPC 100003/2 on 192.168.2.54
    Looking up port of RPC 100005/1 on 192.168.2.54
    VFS: Mounted root (nfs filesystem) on device 0:14.
    Freeing init memory: 144K
    Warning: unable to open an initial console.
    init: cannot find '/system/bin/sgx/rc.pvr', disabling 'pvr'
    init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
    # init: untracked pid 1730 exited
    init: untracked pid 1750 exited
    init: untracked pid 1756 exited
    init: untracked pid 1762 exited
    init: untracked pid 1768 exited
    init: untracked pid 1774 exited
    init: untracked pid 1780 exited
    init: untracked pid 1786 exited

    #
    #
    # init: untracked pid 1792 exited

    init: untracked pid 1798 exited
    #
    # logcat
    I/DEBUG   ( 1727): debuggerd: Dec 28 2011 12:16:22
    I/Vold    ( 1725): Vold 2.1 (the revenge) firing up
    D/Vold    ( 1725): USB mass storage support is not enabled in the kernel
    D/Vold    ( 1725): usb_configuration switch is not enabled in the kernel
    I/Netd    ( 1726): Netd 1.0 starting
    D/Vold    ( 1725): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
    D/AndroidRuntime( 1729):
    D/AndroidRuntime( 1729): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1729): CheckJNI is ON
    W/dalvikvm( 1729): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1729): JNI_CreateJavaVM failed
    I/        ( 1750): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1750): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1750): setMode(NORMAL)
    I/CameraService( 1750): CameraService started (pid=1750)
    I/AudioFlinger( 1750): AudioFlinger's thread 0xc630 ready to run
    D/AndroidRuntime( 1751):
    D/AndroidRuntime( 1751): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1751): CheckJNI is ON
    W/dalvikvm( 1751): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1751): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1756): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1756): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1756): setMode(NORMAL)
    I/CameraService( 1756): CameraService started (pid=1756)
    I/AudioFlinger( 1756): AudioFlinger's thread 0xc630 ready to run
    D/AndroidRuntime( 1761):
    D/AndroidRuntime( 1761): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1761): CheckJNI is ON
    W/dalvikvm( 1761): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1761): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1762): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1762): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1762): setMode(NORMAL)
    I/CameraService( 1762): CameraService started (pid=1762)
    I/AudioFlinger( 1762): AudioFlinger's thread 0xc5d0 ready to run
    D/AndroidRuntime( 1767):
    D/AndroidRuntime( 1767): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1767): CheckJNI is ON
    W/dalvikvm( 1767): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1767): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1768): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1768): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1768): setMode(NORMAL)
    I/CameraService( 1768): CameraService started (pid=1768)
    I/AudioFlinger( 1768): AudioFlinger's thread 0xc630 ready to run
    D/AndroidRuntime( 1773):
    D/AndroidRuntime( 1773): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1773): CheckJNI is ON
    W/dalvikvm( 1773): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1773): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1774): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1774): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1774): setMode(NORMAL)
    I/CameraService( 1774): CameraService started (pid=1774)
    I/AudioFlinger( 1774): AudioFlinger's thread 0xc600 ready to run
    D/AndroidRuntime( 1779):
    D/AndroidRuntime( 1779): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1779): CheckJNI is ON
    W/dalvikvm( 1779): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1779): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1780): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1780): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1780): setMode(NORMAL)
    I/CameraService( 1780): CameraService started (pid=1780)
    I/AudioFlinger( 1780): AudioFlinger's thread 0xc5d0 ready to run
    D/AndroidRuntime( 1785):
    D/AndroidRuntime( 1785): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1785): CheckJNI is ON
    W/dalvikvm( 1785): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1785): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1786): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1786): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1786): setMode(NORMAL)
    I/CameraService( 1786): CameraService started (pid=1786)
    I/AudioFlinger( 1786): AudioFlinger's thread 0xc5d0 ready to run
    D/AndroidRuntime( 1791):
    D/AndroidRuntime( 1791): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1791): CheckJNI is ON
    W/dalvikvm( 1791): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1791): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1792): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1792): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1792): setMode(NORMAL)
    I/CameraService( 1792): CameraService started (pid=1792)
    I/AudioFlinger( 1792): AudioFlinger's thread 0xc5d0 ready to run
    D/AndroidRuntime( 1797):
    D/AndroidRuntime( 1797): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1797): CheckJNI is ON
    W/dalvikvm( 1797): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1797): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1798): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1798): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1798): setMode(NORMAL)
    I/CameraService( 1798): CameraService started (pid=1798)
    I/AudioFlinger( 1798): AudioFlinger's thread 0xc600 ready to run
    D/AndroidRuntime( 1803):
    D/AndroidRuntime( 1803): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1803): CheckJNI is ON
    W/dalvikvm( 1803): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1803): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1804): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1804): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1804): setMode(NORMAL)
    I/CameraService( 1804): CameraService started (pid=1804)
    I/AudioFlinger( 1804): AudioFlinger's thread 0xc630 ready to run
    init: untracked pid 1804 exited
    D/AndroidRuntime( 1810):
    D/AndroidRuntime( 1810): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1810): CheckJNI is ON
    W/dalvikvm( 1810): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1810): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1811): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1811): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1811): setMode(NORMAL)
    I/CameraService( 1811): CameraService started (pid=1811)
    I/AudioFlinger( 1811): AudioFlinger's thread 0xc630 ready to run
    init: untracked pid 1811 exited
    D/AndroidRuntime( 1816):
    D/AndroidRuntime( 1816): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1816): CheckJNI is ON
    W/dalvikvm( 1816): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1816): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1817): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1817): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1817): setMode(NORMAL)
    I/CameraService( 1817): CameraService started (pid=1817)
    I/AudioFlinger( 1817): AudioFlinger's thread 0xc5d0 ready to run
    init: untracked pid 1817 exited
    D/AndroidRuntime( 1822):
    D/AndroidRuntime( 1822): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1822): CheckJNI is ON
    W/dalvikvm( 1822): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1822): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1823): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1823): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1823): setMode(NORMAL)
    I/CameraService( 1823): CameraService started (pid=1823)
    I/AudioFlinger( 1823): AudioFlinger's thread 0xc630 ready to run
    init: untracked pid 1823 exited
    D/AndroidRuntime( 1828):
    D/AndroidRuntime( 1828): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1828): CheckJNI is ON
    W/dalvikvm( 1828): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1828): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died
    I/        ( 1829): ServiceManager: 0xad50
    W/AudioHardwareInterface( 1829): Using stubbed audio hardware. No sound will be produced.
    D/AudioHardwareInterface( 1829): setMode(NORMAL)
    I/CameraService( 1829): CameraService started (pid=1829)
    I/AudioFlinger( 1829): AudioFlinger's thread 0xc630 ready to run
    init: untracked pid 1829 exited
    D/AndroidRuntime( 1834):
    D/AndroidRuntime( 1834): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 1834): CheckJNI is ON
    W/dalvikvm( 1834): JNI_CreateJavaVM failed
    E/AndroidRuntime( 1834): JNI_CreateJavaVM failed
    I/ServiceManager( 1724): service 'media.audio_flinger' died
    I/ServiceManager( 1724): service 'media.audio_policy' died
    I/ServiceManager( 1724): service 'media.player' died
    I/ServiceManager( 1724): service 'media.camera' died

    Thanks and Regards

    Ranjan

  • Hi Ranjan,

    Gngerbread should also work with 2.6.32 kernel.

    Please enable ashmem (CONFIG_ASHMEM) driver along with staging drivers and git it a try.

    Regards,

    Pankaj Bharadiya

     

  • Hi Pankaj,

    As you said , I explored the kernel sources , but i didnt found any option in kernel for enabling (CONFIG_ASHMEM) driver. also i have enabled the android stagging drivers.

    well are there any patches to be applied for linux 2.6.32_rc2 kernel ? if so, where can i find it ?

    Regards D.Ranjan