This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H264: minimum resolution

Hello!

I use encoder 2.30.00.3.
From SPRUEU9B (H.264 Base/Main/Hight Profile Encoder for DM365/DM368 User's Giude June 2011) :

Version 02.00.00.xx also supports version 1.1 standard mode as a
backward compatible option. This can be enabled by setting
encodingPreset = XDM_USER_DEFINED and encQuality = 0/1. It
enables application that needs low-resolution encoding, lesser EDMA
channels or some specific tools like perceptual rate control.

Feature     Version 1.1 - Gen 1       Version 2.0 - Platinum
Resolution  Min - 128 x 96            Min - 320 x 128
            Max - 2k x 2k             Max - Current (2k x 2k)

Question - if I work with resolution 160x1024 need I use version 1.1 or I can use Platinum?

Thank you and excuse me for my bad english.