Other Parts Discussed in Thread: AM1808
Hi,
I am measuring the power consumption of am1808 EVM "TMDXEVMWIFI1808" with wattson adapter and I am little confused why I get so huge readings. So far I have disabled these from defconfig:
-Ethernet
-SATA
-sound card
-HID devices
-USB
-EEPROM
Disabling these takes the power consumption into half of the default configuration, but I still get a power consumption of 900 mW in SOM-M1.

In power spreadsheet and Wiki article it says that typical 300 MHz power consumption is 267 mW. I understand that regulators , SDIO, MMC and UARTs take their own share, but is there some part of SOM-M1 that is waisting huge amounts of power?
Kind regards, Tuomas