Other Parts Discussed in Thread: THS7303
hi
i m using dm365 and trying to insert mt9v113 support
here is modification
struct mt9v113_platform_data mt9v113_pdata = {
//.master = "vpss_master",
//.power_set = 0,,
//.priv_data_set =0, ,
//.ifparm = 0,//mt9v113_ifparm,
/* Some interface dependent params */
.clk_polarity = 0, /* data clocked out on falling edge */
.hs_polarity = 1, /* 0 - Active low, 1- Active high */
.vs_polarity = 1, /* 0 - Active low, 1- Active high */
};
static struct v4l2_input mt9v113_inputs[] = {
{
.index = 0,
.name = "Camera",
.type = V4L2_INPUT_TYPE_CAMERA,
}
};
static struct vpfe_subdev_info vpfe_sub_devs[] = {
#if defined(CONFIG_VIDEO_MT9V113) || defined(CONFIG_VIDEO_MT9V113_MODULE)
{
.module_name = "mt9v113",
//.is_camera = 1,
.grp_id = VPFE_SUBDEV_MT9V113,
.num_inputs = ARRAY_SIZE(mt9v113_inputs),
.routes = 0,
.can_route = 1,
.inputs = mt9v113_inputs,
.ccdc_if_params = {
.if_type = VPFE_YCBCR_SYNC_8,
.hdpol = VPFE_PINPOL_POSITIVE,
.vdpol = VPFE_PINPOL_POSITIVE,
},
.board_info = {
I2C_BOARD_INFO("mt9v113",0x3c),//MT9V113_I2C_ADDR ),
// this is for PCLK rising edge /
.platform_data = &mt9v113_pdata,
},
}
#endif
};
booting info as
i2c /dev entries driver
Linux video capture interface: v2.00
ths7303 1-002c: chip found @ 0x58 (DaVinci I2C adapter)
mt9v113: chip id mismatch read 0x0, expecting 0x2280
vpfe_init
vpfe-capture: vpss clock vpss_master enabled
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
i2c i2c-1: Failed to register i2c client mt9v113 at 0x3c (-16)
vpfe-capture vpfe-capture: v4l2 sub device mt9v113 register fails
No sub devices registered
vpfe-capture: vpfe capture clocks disabled
vpfe_register_ccdc_device: DM365 ISIF
dm365_isif: probe of dm365_isif failed with error -22
thanxx
kailash