This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

When can I download the DM6467 720p Encoder version 01.21.00.02



Hi all,

The link :http://e2e.ti.com/support/embedded/multimedia_software_codecs/f/356/t/98518.aspx

said  Ti will release the DM6467 encoder version 01.21.00.02.

I wanna konw when can I download it;

because i have difficulties in dealing with problems , I need encode H264 using Ti's 720pCodec(not 1080pVersion) to generate multiple slices  based on number bytes per slice ,The 1080pCodec can do that ,but for me it is not proper.

Thank anybody help me ,thank you very much.

Neo Guan