Part Number: AM62P
Hello Ti experts,
This is current state of my booting procedure with different setups mentioned in image above. As per the above image I've 2 questions and they are:
1. While booting Falcon mode boot in eMMC and the SD Card, the time required to boot using eMMC should be technically less than time required to boot from SD Card, Correct is I'm wrong. But, in my case why is time required for booting the same in both SD Card as well as eMMC in Falcon mode?
2. When used InitRAMfs in Falcon boot, the boot-time is increased, why is this happening?
Regards,
Aditya T