This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: AM3352BZCZ60 Uboot SPL Could not Load Uboot from MT29F4G08ABBDAHC-IT NAND flash

Part Number: AM3352

Hey, We uses AM3352BZCZ60 process with the MT29F4G08ABBDAHC (8G Flash)

It has UBI filesystem. After program the unit, it could not boot automatically.

but, I could boot through UART boot, or tftp kernel to boot the system. But it coud not boot automatically  after power up.

It seems that SPL could not load uboot ( first volume of images). 

here are all configuration settings in SPL. (these configuration settings are match to the settings used in linux kern)

#define M_NAND_GPMC_CONFIG1    0x00000800
#define M_NAND_GPMC_CONFIG2    0x00050500 
#define M_NAND_GPMC_CONFIG3    0x00050401 
#define M_NAND_GPMC_CONFIG4    0x04000600
#define M_NAND_GPMC_CONFIG5    0x00070909 
#define M_NAND_GPMC_CONFIG6    0x84000000 
#define M_NAND_GPMC_CONFIG7    0x00000f48

I even tried to create a debug code to read flash ID using readb(). it could not get response. 

I would be appreciated your helps