Other Parts Discussed in Thread: OMAP-L138, OMAPL138
can someone from TI please post a complete list of docs (links) concerning retargeting these drivers for new hardware:
- biospsp
- edma3
- dsplink
- dspbios
and for the sake of others, though I already have these working:
- UBL
- u-boot
- linux kernel
I'm working within the linux dev environment as much as possible (though with the current OMAP-L138 SDK, I need to build UBL in windows with CCS).
This stuff is scattered all over the place, and often it's just a matter of reading the source, but then the question is, which source, where, and what's the recommended way to create a new platform?
Thanks.