Other Parts Discussed in Thread: AM1808, OMAP-L138, AM1810
Hi,
I follow the steps of the "SDK Setup Script" (http://processors.wiki.ti.com/index.php/SDK_Setup_Script) to build SDK environment.
At the end section "Load uboot Script", it would popup a minicom window.
But it would occur error, the below are the error messages.
Booting with TI UBL
Device OPP (456MHz, 1.3V)SD/MMC Boot failed.
How could I do to avoid this error?
The follow are my related environment.
- AM1808 development kit.
- OS: Ubuntu 10.04 LTS
- SDK version: ti-sdk-am180x-evm-05.03.02.00-Linux-x86-Install
Thanks a lot.
Sincerely,
Carl