This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: EE tuning does not seem to affect image on target

Part Number: TDA4VM

Hi Gang,

I'm trying to enable the EE tuning on the target but it doesn't seem to be applied.

What I did so far:

  • Generated the tuning.

  • Added it to the rest of the files.

  • Added the path in generate_dcc.sh:

    $DCC_TOOL_PATH/dcc_gen_linux ar0239_viss_ee_dcc.xml

  • Executed the script.

I also followed the step mentioned in the documentation:

Navigate to /opt/edgeai-tiovx-modules/src/tiovx_viss_module.c (around line 73) and enable ee_mode by replacing it with:

obj->params.fcp[0].ee_mode = TIVX_VPAC_VISS_EE_MODE_Y8;

However, I don't see any difference in the output image compared to before adding the tuning.

Am I missing something in the process, or is there anything else that needs to be enabled for the EE tuning to take effect?

Thanks in advance for the help.

Regards,
Ivan

  • Hi  ,

    This is the tuning I generated with the tool.

    <?xml version="1.0" encoding="utf-8"?>
    <IPIPE_EE_xml xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xsd="http://www.w3.org/2001/XMLSchema">
    	<!--this is comment-->
    	<dcc_name>ipipe_ee</dcc_name>
    	<dcc_header>
    		<camera_module_id>     239 </camera_module_id>
    		<dcc_descriptor_id>   16 </dcc_descriptor_id>
    		<algorithm_vendor_id>  1 </algorithm_vendor_id>
    		<tunning_tool_version> 0 </tunning_tool_version>
    	</dcc_header>
    	<!--=======================================================================-->
    	<typedef>
    		<iss_ipipe_ee type="struct">
    			<enable type="uint16"> </enable> <!-- enable/disable ipipe edge enhancer: 0,1 -->
    			<halo_reduction_enable type="uint16"> </halo_reduction_enable> <!-- enable/disable ipipe es halo reduction: 0,1 -->
    			<ee_2d_filter_coeff type="int16[9]"> </ee_2d_filter_coeff> <!-- 2d filter coefficieints: S10 -->
    			<merge_select type="uint16"> </merge_select> <!-- select merge type(TRM is wrong):0(EE + ES),1(Max (EE, ES)) -->
    			<shift_amount type="uint16"> </shift_amount> <!-- shift right amount: U6 -->
    			<threshold_before_lut type="uint16"> </threshold_before_lut> <!-- threshold (shrink) before lut: U10 -->
    			<edge_sharpener_gain type="uint16"> </edge_sharpener_gain> <!-- edge sharpener gain: U12Q6 -->
    			<edge_sharpener_hpf_low_thresh type="uint16"> </edge_sharpener_hpf_low_thresh> <!-- edge sharpener threshold low (shrink): U16Q6 -->
    			<edge_sharpener_hpf_high_thresh type="uint16"> </edge_sharpener_hpf_high_thresh> <!-- dge sharpener threshold high: U10 -->
    			<edge_sharpener_gradient_gain type="uint16"> </edge_sharpener_gradient_gain> <!-- edge sharpener gradient gain: U8Q6 -->
    			<edge_sharpener_gradient_offset type="uint16"> </edge_sharpener_gradient_offset> <!-- edge sharpener gradient offset: U10 -->
    			<edge_intensity_lut type="int16[4096]"> </edge_intensity_lut> <!-- edge intensity lut: S13 -->
    		</iss_ipipe_ee>
    	</typedef>
    	<!--=======================================================================-->
    	
    	<use_case val="1023">
    		<n-space>
    		
    			<region0 class="0">
    				<colortemperature val="2" min="0" max="20000">  </colortemperature>
    				<exposure val="1" min="0" max="10000000">  </exposure>
    				<gain val="0" min="0" max="1024">  </gain>
    			</region0>
    		
    		</n-space>
    		
    		<parameter_package>           
    			<ipipe_ee_dcc type="iss_ipipe_ee">
    			{
    				1, // enable
    				0, // halo_reduction_enable
    				{ 
    					-2, -6, -10,
    					-6, 0, 12,
    					-10, 12, 48
    
    				}, // ee_2d_filter_coeff
    				0, // merge_select
    				3, // shift_amount
    				160, // threshold_before_lut
    				0, // edge_sharpener_gain
    				10240, // edge_sharpener_hpf_low_thresh
    				512, // edge_sharpener_hpf_high_thresh
    				96, // edge_sharpener_gradient_gain
    				384, // edge_sharpener_gradient_offset
    				{ // edge_intensity_lut
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -512 -512 -512
                    -512 -511 -510 -510
                    -509 -508 -507 -506
                    -506 -505 -504 -503
                    -502 -502 -501 -500
                    -499 -498 -498 -497
                    -496 -495 -494 -494
                    -493 -492 -491 -490
                    -490 -489 -488 -487
                    -486 -486 -485 -484
                    -483 -482 -482 -481
                    -480 -479 -478 -478
                    -477 -476 -475 -474
                    -474 -473 -472 -471
                    -470 -470 -469 -468
                    -467 -466 -466 -465
                    -464 -463 -462 -462
                    -461 -460 -459 -458
                    -458 -457 -456 -455
                    -454 -454 -453 -452
                    -451 -450 -450 -449
                    -448 -447 -446 -446
                    -445 -444 -443 -442
                    -442 -441 -440 -439
                    -438 -438 -437 -436
                    -435 -434 -434 -433
                    -432 -431 -430 -430
                    -429 -428 -427 -426
                    -426 -425 -424 -423
                    -422 -422 -421 -420
                    -419 -418 -418 -417
                    -416 -415 -414 -414
                    -413 -412 -411 -410
                    -410 -409 -408 -407
                    -406 -406 -405 -404
                    -403 -402 -402 -401
                    -400 -399 -398 -398
                    -397 -396 -395 -394
                    -394 -393 -392 -391
                    -390 -390 -389 -388
                    -387 -386 -386 -385
                    -384 -383 -382 -382
                    -381 -380 -379 -378
                    -378 -377 -376 -375
                    -374 -374 -373 -372
                    -371 -370 -370 -369
                    -368 -367 -366 -366
                    -365 -364 -363 -362
                    -362 -361 -360 -359
                    -358 -358 -357 -356
                    -355 -354 -354 -353
                    -352 -351 -350 -350
                    -349 -348 -347 -346
                    -346 -345 -344 -343
                    -342 -342 -341 -340
                    -339 -338 -338 -337
                    -336 -335 -334 -334
                    -333 -332 -331 -330
                    -330 -329 -328 -327
                    -326 -326 -325 -324
                    -323 -322 -322 -321
                    -320 -319 -318 -318
                    -317 -316 -315 -314
                    -314 -313 -312 -311
                    -310 -310 -309 -308
                    -307 -306 -306 -305
                    -304 -303 -302 -302
                    -301 -300 -299 -298
                    -298 -297 -296 -295
                    -294 -294 -293 -292
                    -291 -290 -290 -289
                    -288 -287 -286 -286
                    -285 -284 -283 -282
                    -282 -281 -280 -279
                    -278 -278 -277 -276
                    -275 -274 -274 -273
                    -272 -271 -270 -270
                    -269 -268 -267 -266
                    -266 -265 -264 -263
                    -262 -262 -261 -260
                    -259 -258 -258 -257
                    -256 -255 -254 -254
                    -253 -252 -251 -250
                    -250 -249 -248 -247
                    -246 -246 -245 -244
                    -243 -242 -242 -241
                    -240 -239 -238 -238
                    -237 -236 -235 -234
                    -234 -233 -232 -231
                    -230 -230 -229 -228
                    -227 -226 -226 -225
                    -224 -223 -222 -222
                    -221 -220 -219 -218
                    -218 -217 -216 -215
                    -214 -214 -213 -212
                    -211 -210 -210 -209
                    -208 -207 -206 -206
                    -205 -204 -203 -202
                    -202 -201 -200 -199
                    -198 -198 -197 -196
                    -195 -194 -194 -193
                    -192 -191 -190 -190
                    -189 -188 -187 -186
                    -186 -185 -184 -183
                    -182 -182 -181 -180
                    -179 -178 -178 -177
                    -176 -175 -174 -174
                    -173 -172 -171 -170
                    -170 -169 -168 -167
                    -166 -166 -165 -164
                    -163 -162 -162 -161
                    -160 -159 -158 -158
                    -157 -156 -155 -154
                    -154 -153 -152 -151
                    -150 -150 -149 -148
                    -147 -146 -146 -145
                    -144 -143 -142 -142
                    -141 -140 -139 -138
                    -138 -137 -136 -135
                    -134 -134 -133 -132
                    -131 -130 -130 -129
                    -128 -127 -126 -126
                    -125 -124 -123 -122
                    -122 -121 -120 -119
                    -118 -118 -117 -116
                    -115 -114 -114 -113
                    -112 -111 -110 -110
                    -109 -108 -107 -106
                    -106 -105 -104 -103
                    -102 -102 -101 -100
                    -99 -98 -98 -97
                    -96 -95 -94 -94
                    -93 -92 -91 -90
                    -90 -89 -88 -87
                    -86 -86 -85 -84
                    -83 -82 -82 -81
                    -80 -79 -78 -78
                    -77 -76 -75 -74
                    -74 -73 -72 -71
                    -70 -70 -69 -68
                    -67 -66 -66 -65
                    -64 -63 -62 -62
                    -61 -60 -59 -58
                    -58 -57 -56 -55
                    -54 -54 -53 -52
                    -51 -50 -50 -49
                    -48 -47 -46 -46
                    -45 -44 -43 -42
                    -42 -41 -40 -39
                    -38 -38 -37 -36
                    -35 -34 -34 -33
                    -32 -31 -30 -30
                    -29 -28 -27 -26
                    -26 -25 -24 -23
                    -22 -22 -21 -20
                    -19 -18 -18 -17
                    -16 -15 -14 -14
                    -13 -12 -11 -10
                    -10 -9 -8 -7
                    -6 -6 -5 -4
                    -3 -2 -2 -1
                    0 1 2 2
                    3 4 5 6
                    6 7 8 9
                    10 10 11 12
                    13 14 14 15
                    16 17 18 18
                    19 20 21 22
                    22 23 24 25
                    26 26 27 28
                    29 30 30 31
                    32 33 34 34
                    35 36 37 38
                    38 39 40 41
                    42 42 43 44
                    45 46 46 47
                    48 49 50 50
                    51 52 53 54
                    54 55 56 57
                    58 58 59 60
                    61 62 62 63
                    64 65 66 66
                    67 68 69 70
                    70 71 72 73
                    74 74 75 76
                    77 78 78 79
                    80 81 82 82
                    83 84 85 86
                    86 87 88 89
                    90 90 91 92
                    93 94 94 95
                    96 97 98 98
                    99 100 101 102
                    102 103 104 105
                    106 106 107 108
                    109 110 110 111
                    112 113 114 114
                    115 116 117 118
                    118 119 120 121
                    122 122 123 124
                    125 126 126 127
                    128 129 130 130
                    131 132 133 134
                    134 135 136 137
                    138 138 139 140
                    141 142 142 143
                    144 145 146 146
                    147 148 149 150
                    150 151 152 153
                    154 154 155 156
                    157 158 158 159
                    160 161 162 162
                    163 164 165 166
                    166 167 168 169
                    170 170 171 172
                    173 174 174 175
                    176 177 178 178
                    179 180 181 182
                    182 183 184 185
                    186 186 187 188
                    189 190 190 191
                    192 193 194 194
                    195 196 197 198
                    198 199 200 201
                    202 202 203 204
                    205 206 206 207
                    208 209 210 210
                    211 212 213 214
                    214 215 216 217
                    218 218 219 220
                    221 222 222 223
                    224 225 226 226
                    227 228 229 230
                    230 231 232 233
                    234 234 235 236
                    237 238 238 239
                    240 241 242 242
                    243 244 245 246
                    246 247 248 249
                    250 250 251 252
                    253 254 254 255
                    256 257 258 258
                    259 260 261 262
                    262 263 264 265
                    266 266 267 268
                    269 270 270 271
                    272 273 274 274
                    275 276 277 278
                    278 279 280 281
                    282 282 283 284
                    285 286 286 287
                    288 289 290 290
                    291 292 293 294
                    294 295 296 297
                    298 298 299 300
                    301 302 302 303
                    304 305 306 306
                    307 308 309 310
                    310 311 312 313
                    314 314 315 316
                    317 318 318 319
                    320 321 322 322
                    323 324 325 326
                    326 327 328 329
                    330 330 331 332
                    333 334 334 335
                    336 337 338 338
                    339 340 341 342
                    342 343 344 345
                    346 346 347 348
                    349 350 350 351
                    352 353 354 354
                    355 356 357 358
                    358 359 360 361
                    362 362 363 364
                    365 366 366 367
                    368 369 370 370
                    371 372 373 374
                    374 375 376 377
                    378 378 379 380
                    381 382 382 383
                    384 385 386 386
                    387 388 389 390
                    390 391 392 393
                    394 394 395 396
                    397 398 398 399
                    400 401 402 402
                    403 404 405 406
                    406 407 408 409
                    410 410 411 412
                    413 414 414 415
                    416 417 418 418
                    419 420 421 422
                    422 423 424 425
                    426 426 427 428
                    429 430 430 431
                    432 433 434 434
                    435 436 437 438
                    438 439 440 441
                    442 442 443 444
                    445 446 446 447
                    448 449 450 450
                    451 452 453 454
                    454 455 456 457
                    458 458 459 460
                    461 462 462 463
                    464 465 466 466
                    467 468 469 470
                    470 471 472 473
                    474 474 475 476
                    477 478 478 479
                    480 481 482 482
                    483 484 485 486
                    486 487 488 489
                    490 490 491 492
                    493 494 494 495
                    496 497 498 498
                    499 500 501 502
                    502 503 504 505
                    506 506 507 508
                    509 510 510 511
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
                    512 512 512 512
    
    				}
    			}
    			</ipipe_ee_dcc>
    		</parameter_package>
    		
    	</use_case>
    	
    	<!--=====================================================================-->
    </IPIPE_EE_xml>
    

  • Hi Ivan,

    Is this on SK-TDA4VM EVM (https://www.ti.com/tool/SK-TDA4VM)?

    Which version of the SDk do you use?

  • Hi Gang,

    Is this on SK-TDA4VM EVM (https://www.ti.com/tool/SK-TDA4VM)?

    Which version of the SDk do you use?

    Yes, the version is ti-processor-sdk-rtos-j721e-evm-11_01_00_04

  • There was one known EE issue for 11.01 on J722S in this thread below.

    I’m using J721E - will it be the same there? Is there an official fix, or will I have to revert to an older commit?

    Apart from this commit, does anything else need to be changed in any other file?
    I’m not entirely sure where these lines are coming from:

    What I’ve done so far I described above.

  • Hi Ivan,

    I’m using J721E - will it be the same there? Is there an official fix, or will I have to revert to an older commit?

    I tested the latest "ti-processor-sdk-rtos-j721e-evm-11_02_00_06" and seems to have similar EE issues.

    It might be either the same issue as j722s or a different one.
    I will have to check integrally.

  • Hi Gang,

    You may try rolling back this commit.

    I tried with this commit, but I didn’t see the sharpness being applied again.

  • Hi Ivan,

    I tried with this commit, but I didn’t see the sharpness being applied again.

    I did some tests on J721E RTOS SDK 11.02 and 11.01.
    Rolling back the commit enables EE for TIVX_VPAC_VISS_EE_MODE_Y8 mode on both.

    I am not familiar with the edgeai s/w stack and not aware of any s/w changes there.
    We just have a bug filed for the same issue on edgeai/am62a.
    If rolling back the viss kernel commit does not work for you, we will have to wait for the resolution of the bug.