This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Windows Client for Echo server program



Hello friends,

I  am testing Echo Server Application example that comes along with StarterWare. I created a project in visual studio 2005 based on client.c program but did not compile because this program meant for Linux Host  and needs to be modified so that I can use Windows Host as client.

Can any body please suggest me what modifications shall I have to do. Or is there any Windows Host client.c program available for StarterWare?

Thank you

regards,

Mahesh

  • Hi Mahesh,

    The Host Client client.c program for Windows is not available with StarterWare.

    Regards

    Sujith.

  • Dear friend,

    Is it a pre-requisite that the host PC givshould always be Linux based if I want to use StarterWare? Can't I use Windows PC?

    Is it a worthy idea to try to convert the en client.c program for Windows and work with it. Because some part of my project is already implemented in Visual studio 2005 and I want to add network TCP/IP functionality to it and use it with StarterWare.

    I am waiting for your valuable suggestion in this regard.

    Regards,

    Mahesh

  • Dear friend,

    - Is it a pre-requisite that the host PC should always be Linux based if I want to use StarterWare? Can't I use Windows PC?

    - Is it a worthy idea to try to convert the en client.c program for Windows and work with it. Because some part of my project is already implemented in Visual studio 2005 and I want to add network TCP/IP functionality to it and use it with StarterWare.

    - MATLAB also have support for TCP/IP and UDP sockets on Windows. Should I consider TCP/IP or UDP stack implemented in StarterWare generic such that I can I try with MATLAB also.

    Regards,

    Mahesh

  • Hi Mahesh,

    StarterWare you can install on both Windows and Linux PCs. There are GCC makefile project examples which you can use in Linux as well as CCS/IAR projects which you can import in Windows installations.

    Also, StarterWare  implements lwIP, a light weight IP stack, which is generic. It doesnt depend on the host PC.

    But the client program given in /host_apps, is only for linux. However, you can develop your own client program for Windows and test it with StarterWare, by loading enet_echo executable on your target EVM.

    Also, you can try loading enet_lwip program onto your target and access the embedded webpage from your Windows PC.

    http://processors.wiki.ti.com/index.php/StarterWare_02.00.00.05_User_Guide#Embedded_Web_Server_application    will give you the details.

    Cheers,

    Sujith.

     

  • Mahesh,

    I am also using an L138 EVM and want to get the enet_echo working with a Windows program rather than the supplied Linux enet client. Did you find a solution?

    Thanks,

    Keith.