Can DVSDK 4.03 be used on BeagleBoard xM.
What changes need to be done to make DVSDK work on BeagleBoard xM.
Thanks,
Anand
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can DVSDK 4.03 be used on BeagleBoard xM.
What changes need to be done to make DVSDK work on BeagleBoard xM.
Thanks,
Anand
Anand,
DVSDK 4.03 Official support for beagle board is not there. So this release is not ported to BeagleBoard. it would be great if some one from communicate can contribute to this.
I am not familiar with the differences but i could put it like this
The starting place could be http://processors.wiki.ti.com/index.php/DVSDK_4.x_FAQ#How_to_build_and_install_DVSDK_4.01_on_BeagleBoard-xM
As the older version of DVSDK is ported to BeagleBoard, just identify the differences and apply those on the DVSDK 4.03.
Please have a look at the other post http://e2e.ti.com/support/embedded/linux/f/354/t/155977.aspx#594802, this post does not have any solution, but marks that some one else also has same question.
Thanks & Regards,
Velan
Hi Velan,
Just wanna ask if there are good news for the BB-xM porting using DVSDK4.03 since I am dying. lol
Thanks.