This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NAND AT CHIP SELECT 7

hi all,

I'm trying to do configuration for nand at chip select 7 in u-boot code!

mem.h , mem.c files i have modified all gpmc registers according to our timings but one trick in mem.h file

#if defined(CONFIG_ENV_IS_IN_NAND)

#define NAND_CS 0

else

#define NAND_CS 1

For above #defines, so i need to use chip select 7

so when i changed above

#if defined(CONFIG_ENV_IS_IN_NAND)

#define NAND_CS 7

#endif

And also in omap3_beagle.h

NAND_BASE

In board/ti/beagle/beagle.h

MUX_PIN(NCS7) (IDIS | PTU|EN|M0);

By above changes after u-boot is not booting!!!!!!!!!!!!!

BUT when i make again that NAND_CS 0

It is booting.............

Can anyone share there thoughts on this issue?

Regards,

santosh vastrad