Part Number: TDA4VM
Hi Team,
After creating the SD card partition, I followed the run instructions from the user guide. However, when I power on the board, I see the following boot prints. Could someone please help me resolve this issue?
Regards,
Sai Teja
U-Boot SPL 2025.01-00773-gdf1fe2382304 (Dec 24 2025 - 07:50:42 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.2.8--v11.02.08 (Fancy Rat)')
Trying to boot from MMC2
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Loading Environment from nowhere... OK
Starting ATF on ARM64 core...
NOTICE: BL31: v2.13.0(release):v2.13.0-259-ge0c4d3903b-dirty
NOTICE: BL31: Built : 07:01:36, Jul 1 2025
I/TC:
I/TC: OP-TEE version: 4.7.0-47-ga9690ae39 (gcc version 13.4.0 (GCC)) #1 Thu Aug 7 15:25:10 UTC 2025 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000b '11.2.8--v11.02.08 (Fancy Rat)')
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: EIP76D TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: HUK Initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2025.01-00773-gdf1fe2382304-dirty (Dec 24 2025 - 07:50:42 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.2.8--v11.02.08 (Fancy Rat)')
DM ABI: 3.0 (firmware ver 0x000b 'PSDK.11.02.00.07--v11.02.07' patch_ver: 7)
Detected: J7X-BASE-CPB rev A
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
Skipping authentication on GP device
Skipping authentication on GP device
U-Boot 2025.01-00773-gdf1fe2382304-dirty (Dec 24 2025 - 07:50:42 +0000)
SoC: J721E SR1.1 GP
Model: Texas Instruments J721e EVM
Board: J721EX-PM2-SOM rev A
DRAM: 2 GiB (total 4 GiB)
Core: 151 devices, 37 uclasses, devicetree: separate
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev A
Detected: J7X-VSC8514-ETH rev E2
Net: am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1
eth0: ethernet@46000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
907 bytes read in 3 ms (294.9 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
gpio: pin gpio@22_17 (gpio 281) value is 1
gpio: pin gpio@22_16 (gpio 280) value is 0
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
Failed to load '/lib/firmware/j7-mcu-r5f0_1-fw'
1519116 bytes read in 37 ms (39.2 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 1519116 bytes: Success!
396348 bytes read in 13 ms (29.1 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 396348 bytes: Success!
Failed to load '/lib/firmware/j7-main-r5f1_0-fw'
Failed to load '/lib/firmware/j7-main-r5f1_1-fw'
1342288 bytes read in 33 ms (38.8 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 1342288 bytes: Success!
1342288 bytes read in 33 ms (38.8 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 1342288 bytes: Success!
13049944 bytes read in 275 ms (45.3 MiB/s)
Load Remote Processor 8 with data@addr=0x82000000 13049944 bytes: Success!
20593152 bytes read in 428 ms (45.9 MiB/s)
113998 bytes read in 7 ms (15.5 MiB/s)
Working FDT set to 88000000
Failed to load '/boot/dtb/ti/k3-j721e-evm-ethfw.dtbo'
11720 bytes read in 5 ms (2.2 MiB/s)
failed on fdt_overlay_apply(): FDT_ERR_NOTFOUND
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
Scanning for bootflows in all bootdevs
Seq Method State Uclass Part Name Filename
--- ----------- ------ -------- ---- ------------------------ ----------------
Scanning bootdev 'mmc@4fb0000.bootdev':
Scanning bootdev 'mmc@4f80000.bootdev':
Bus usb@6400000: cdns-usb3-host usb@6400000: DRD version v1 (ID: 0004024e, rev: 00000200)
Register 2000840 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@6400000 for devices... 2 USB Device(s) found
k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 3
ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5