Part Number: AM62P
Other Parts Discussed in Thread: SN74LV1T08
Hi team,
Currently, we are evaluating the USB interface as part of the assessment of a custom board equipped with the AM62P.
As shown in the following figure, the DRVVBUS of the AM62P on the custom board is connected to the input of the SN74LV1T08 (AND gate) via a 10k pull-down resistor.
However, when DRVVBUS is outputting a high level, the expected voltage level is approximately 1.8V, but it only reaches about 0.5V.
On the other hand, removing the pull-down resistor results in the DRVVBUS output voltage being approximately 1.8V.
What could be the cause of the DRVVBUS output level dropping under these conditions?
Is the drive strength setting of the DRVVBUS terminal inappropriate?
Thank you for your support.