This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sitara PRU Uart pin mux question



I need to make a specialized UART that looks for certain timing gaps to indicate message boundaries.  It also has to implement a collision avoidance algorithm.  Ultimately, though, it's still asynchronous like a normal UART.

What I would like to do is implement this using a PRU, and the PRU UART0 in the AM3359x (not the UART on the ARM, I'm talking about the PRU specific UART).

I'm wondering: is it possible to have the pinmux set up so that PRU0 is talking to that uart but can *ALSO* see the RX pin as if it were a GPIO pin set up as an input?