Can someone point me to the documentation of the location of the timer interrupt enable register in the C5515? I can't seem to find it in sprufo2.
Also, section 6.14 Timer Interrupt Aggregation Flag pargraph states:
Note that the corresponding Timer Interrupt Register must also be cleared.
Where is the Timer Interrupt Register documented? Here are the only registers that appear in sprufo1.

Sorry if I've overlooked something simple.