This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fail to capture from composite



Using tms320dm6467 with dvsdk 3.10.00.19

Created capture attributes with values

3,

Capture_Input_COMPOSITE,

-1,

-1,

-1,

-1,

"/dev/video0",

FALSE,

VideoStd_AUTO,

-1,

ColorSpace_YUV422PSEMI,

NULL

Getting fail (return value -1) on call to:

               Capture_detectVideoStd(NULL, &videoStd, &cAttrs);

Running DMAI_DEBUG=2 ./encode

Encode demo started.
@0x00003506:[T:0x4001fcd0] ti.sdo.dmai - [Dmai] Dmai log level set to '2'. Note that calling CERuntime_init after this point may cause unexpected change to DMAI tracing behavior.
@0x00003cdf:[T:0x413d6490] ti.sdo.dmai - [Capture] Composite input selected
@0x00003fe1:[T:0x413d6490] ti.sdo.dmai - [Capture] Checking video standard
@0x00004100:[T:0x413d6490] ti.sdo.dmai - [Capture] VIDIOC_QUERYSTD failed on /dev/video0. Video input connected?
Error: Failed to detect input video standard (-1), input connected?