This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6727B: Source code and build instructions for libraries

Part Number: TMS320C6727B
Other Parts Discussed in Thread: SPRC203, SPRC223, CCSTUDIO

Hi experts,

Could you please provide the source code and build instructions for the following libraries?
Note that the DSP/BIOS version used in the original thread has been updated to V5.33.06.

  • rts67plus.lib (source available, but not sure if it can be used as an equivalent)
    Compiler (C:\ti\C6000 Code Generation Tools 7.3.0\lib)

  • c67xdsplibR.lib (source not available)
    SPRC203 (sprc203\UsingROMApplications\FastRts_DspLib\ROMexamples\c67xdsplib\lib)

  • fastrts67xR.lib (source available, but not sure how to build the library with R)
    SPRC203 (sprc203\UsingROMApplications\FastRts_DspLib\ROMexamples\c67xfastrts\lib)

  • csl_C6727.lib (source available)
    SPRC223 (sprc223\csl_C672x_03_00_09_00\csl_C672x_03_00_09_00\dsp\lib)

  • c672xSystemPatchV2_00_00.lib (no source)
    SPRC203 (sprc203\SystemPatch)

  • lnkrtdx.a67P (no source)
    DSP/BIOS (C:\CCStudio_v3.3\bios_5_ 31_02\packages\ti\bios\lib)

  • bios.a67P (no source)
    DSP/BIOS (C:\CCStudio_v3.3\bios_5_31_02\packages\ti\bios\lib)

  • biosDA700.a67P (no source)
    DSP/BIOS (C:\CCStudio_v3.3\bios_5_31_02\packages\ti\bios\lib)

Best regards,
O.H