This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-LINUX-J721E: Issue with wayland

Part Number: PROCESSOR-SDK-LINUX-J721E

Hi,

     I am using processor sdk linux for J721E  8_06 jacinto. I tried to run Qt application in linux OS and it running fine without error. But when I try to run using a shell script command it shows lot of error relate with wayland like "Failed to create wl_display(No such file or directory)", "qt.qpa.plugin: could not load the qt platform plugin "wayland" in "" even though it was found", "this application failed to start because no Qt platform plugin could be initialized. reinstalling the application etc".  I tried to export qt platform in the shell script. But nothing worked.

 

Regards,

Rejin