Part Number: AM62D-Q1
I am working on an embedded audio processing system built around AM62D. The system is designed to use 4Gb (512MB) of LPDDR4 memory. Can I use an 8Gb memory IC instead and operate the system without making any changes to the software or DDR configuration? What about if the reverse were true, where a 4Gb part is placed and the controller is set to 8Gb density (operating system still only using 4Gb)? I would like to better understand how changing the configured density affects the behavior of the controller (if at all).