Part Number: SK-AM62A-LP
Hello,
We are building the image from SDK 11.01.05.07 with Yocto for SK-AM62A-LP.
We want to activate the watchdog when the A53 CPUs start up, so if possible when u-boot starts up.
The expected action at the end of the watchdog time is a complete system reboot.
To do this, we have added the following fragment.cfg to the u-boot-ti-stagging recipe.
The watchdog behaves as expected in u-boot, but when we start linux kernel only one A53 core starts correctly.
We can compare console_with_fragment.log and console_without_fragment.log .
Have we forgotten something to achieve our requirement ?
Regards,
Benjamin