Part Number: TDA4VEN-Q1
Hi.
On the evaluation board created with reference to the J722S EVM,
power supply interference occurred at startup.
For circuit debugging, when the signal line connected to GPIO1_8 (A26)
of the TDA4VEN was pulled up to VSYS_3V3, VDDSHV0, which is a separate
power supply, powered up in a sequence faster than usual.
Since GPIO1_8 is of the LVCMOS type, it is expected that a DC path is created
to VDDSHV0 through the IO’s P-MOS transistor.
Is the inference correct that GPIO1_8 will serve as a DC path to VDDSHV0
during system startup?
(What is the state of GPIO1_8 at system startup?)