Hi,
When I run saLoopback application with V4l2 based capture (TVP7002). I get following crash. Has anyone encountered same issue? If yes, did anyone tried to find root cause or solution of this problem?
=============================================================================================
------------[ cut here ]------------
WARNING: at kernel/softirq.c:159 local_bh_enable+0x54/0xc4()
Modules linked in: bufferclass_ti omaplfb pvrsrvkm ti81xxhdmi tvp7002 ti81xxvin sii9135 ti81xxvo ti81xxfb vpss syslink ipv6
Backtrace:
[<c0048b58>] (dump_backtrace+0x0/0x110) from [<c036b8d8>] (dump_stack+0x18/0x1c)
r7:00000000 r6:c00712d0 r5:c042e572 r4:0000009f
[<c036b8c0>] (dump_stack+0x0/0x1c) from [<c006bd54>] (warn_slowpath_common+0x54/0x6c)
[<c006bd00>] (warn_slowpath_common+0x0/0x6c) from [<c006bd90>] (warn_slowpath_null+0x24/0x2c)
r9:c04d94bc r8:cb08c880 r7:0000000f r6:c72a1a00 r5:c04b330c
r4:c05047c0
[<c006bd6c>] (warn_slowpath_null+0x0/0x2c) from [<c00712d0>] (local_bh_enable+0x54/0xc4)
[<c007127c>] (local_bh_enable+0x0/0xc4) from [<c0065c58>] (omap_mbox_msg_send+0xcc/0xdc)
r5:c04b330c r4:00000000
[<c0065b8c>] (omap_mbox_msg_send+0x0/0xdc) from [<c02aca90>] (notify_shm_drv_send_event+0x1c8/0x208)
r5:00000001 r4:00000000
[<c02ac8c8>] (notify_shm_drv_send_event+0x0/0x208) from [<c02aa220>] (notify_send_event+0x114/0x26c)
[<c02aa10c>] (notify_send_event+0x0/0x26c) from [<bf18c610>] (vps_fvid2_queue+0x94/0x1cc [vpss])
[<bf18c57c>] (vps_fvid2_queue+0x0/0x1cc [vpss]) from [<bf1955b0>] (capture_queue+0x50/0x64 [vpss])
r8:bf1cd404 r7:60000013 r6:c6fecd80 r5:00000000 r4:c5f6b400
[<bf195560>] (capture_queue+0x0/0x64 [vpss]) from [<bf1cc1c8>] (ti81xxvin_buffer_queue+0x9c/0xe8 [ti81xxvin])
r5:c5fb4000 r4:c5f6b400
[<bf1cc12c>] (ti81xxvin_buffer_queue+0x0/0xe8 [ti81xxvin]) from [<c0283a78>] (videobuf_streamon+0x80/0xd0)
r7:60000013 r6:c5fb41c4 r5:c5fb4104 r4:c6fecd80
[<c02839f8>] (videobuf_streamon+0x0/0xd0) from [<bf1cbc40>] (vidioc_streamon+0x244/0x400 [ti81xxvin])
r7:c5ffd600 r6:00000001 r5:c5fb4000 r4:c5fb4104
[<bf1cb9fc>] (vidioc_streamon+0x0/0x400 [ti81xxvin]) from [<c0279380>] (__video_do_ioctl+0x1618/0x3f34)
r6:40045612 r5:00000000 r4:00000001
[<c0277d68>] (__video_do_ioctl+0x0/0x3f34) from [<c0277b58>] (__video_usercopy+0x2e4/0x428)
[<c0277874>] (__video_usercopy+0x0/0x428) from [<c0277ccc>] (video_ioctl2+0x30/0x38)
[<c0277c9c>] (video_ioctl2+0x0/0x38) from [<c0276d0c>] (v4l2_ioctl+0xe8/0x11c)
r5:c5ffd600 r4:c6fecb80
[<c0276c24>] (v4l2_ioctl+0x0/0x11c) from [<c00d10e4>] (vfs_ioctl+0x28/0x44)
r9:c7172000 r8:beeb5c94 r7:00000003 r6:00000003 r5:c6fecb80
r4:00000000
[<c00d10bc>] (vfs_ioctl+0x0/0x44) from [<c00d17f4>] (do_vfs_ioctl+0x500/0x540)
[<c00d12f4>] (do_vfs_ioctl+0x0/0x540) from [<c00d188c>] (sys_ioctl+0x58/0x7c)
[<c00d1834>] (sys_ioctl+0x0/0x7c) from [<c0044da0>] (ret_fast_syscall+0x0/0x30)
r8:c0044f48 r7:00000036 r6:000124d0 r5:0001215c r4:beeb5c94
---[ end trace 356cb976708ec655 ]---
=============================================================================================
--
Regards,
Krunal