Hello all,
How to initialize uart at u-boot i have added in the board/ti/evm/evm.h as MUX_VAL(CP(GPMC_WAIT2), (IEN | PTU | EN | M2))
Also added the Base address in the include/asm/arch-omap3/omap3.h as #define OMAP34XX_UART4 0x49042000
do i need to do anything to use the uart port at u-boot level .can any help on this .
Thanks,
Ranjith.