Other Parts Discussed in Thread: TMS320C6472
What is the invalid code in the following?
When immediate boot is selected after global reset, the C64x+ megamodule core executes directly
from the internal L2 SRAM address programmed in the DSP_BOOT_ADDRx register. Note: device
operation is undefined if invalid code is address programmed in the DSP_BOOT_ADDRx register.
Executing invalid code may prevent connection by an emulator.
TMS320C6472 Fixed-Point Digital Signal Processor (Rev. G)
http://www.ti.com/lit/ds/sprs612g/sprs612g.pdf
2.4.1 Boot Modes Supported
Best regards,
Daisuke