Hello
I'm using a DSK6455 + 5-6K interface + ADS1274EVM and ADS1282EVM boards, and I'm working with SPI protocol.
The EVM boards use the interrupt on pin J5.15. I think that this pin is wired via 5-6K interface to the GP(6) pin in the 6455 CPU. Please, can you confirm this?
The interrupt GP(6) has asscociated the event number 57. Please, can you confirm this?
Well, my last question, must I program the GPIO module to prepare the external interrupts or is it programmed in the DSK6455 board?. If not, have you got any example?
Thanks and best regards.
Manuel Fernández Ros.