Other Parts Discussed in Thread: ADS7846
Hi Experts,
I have been strugging a few days to put file system on Nand of AM37x EVM board. My Linux kernel uImage can be boot successfully if using host filesystem mapping, NFS on my host PC through Ethernet. The user guide from my SDK package is far from enough. Here is what I did to setup the file system in Nand by following a few user guide links:
1. Since I do not have a sample file system tree or image, I build the target file system using busybox and followed instructions below.
http://processors.wiki.ti.com/index.php/Creating_a_Root_File_System_for_Linux_on_OMAP35x
2. I made jffs2 image by following: http://processors.wiki.ti.com/index.php/Create_a_JFFS2_Target_Image
3. I put the jffs2 image into nand by following http://processors.wiki.ti.com/index.php/Put_JFFS2_Image_to_Flash. Since nand write.trimffs is not working in the SDK U-boot and the latest u-boot does not start with my SDK x-loader, I wrote the jffs2 image from Linux by using flash-eraseall, and nandwrite to /dev/mtd4 which is my nand partition.
4. I booted the board and change the filesystem bootargs as 'setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2'
The Linux boot is stuck after 6 seconds and here is the boot up log below. Please help to give me some clues what could be wrong. Thanks.
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 2.6.37 (cwang@ubuntu) (gcc version 4.3.3 (GCC) ) #36 Mon Jan 9 09:50:17 E2
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP3 EVM
[ 0.000000] Reserving 4194304 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] OMAP3630 ES1.2 (l2cache iva sgx neon isp 192mhz_clk )
[ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64000
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mtdblock4 rw rootfstype=jffs2
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 252MB = 252MB total
[ 0.000000] Memory: 243044k/243044k available, 19100k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc003c000 ( 208 kB)
[ 0.000000] .text : 0xc003c000 - 0xc0520b08 (5011 kB)
[ 0.000000] .data : 0xc0522000 - 0xc06d3920 (1735 kB)
[ 0.000000] NR_IRQS:409
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/1000 MHz
[ 0.000000] omap_hwmod: i2c1: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c2: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c3: softreset failed (waited 10000 usec)
[ 0.000000] Reprogramming SDRC clock to 400000000 Hz
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] GPMC revision 5.0
[ 0.000000] Trying to install interrupt handler for IRQ402
[ 0.000000] Trying to install interrupt handler for IRQ403
[ 0.000000] Trying to install interrupt handler for IRQ404
[ 0.000000] Trying to install interrupt handler for IRQ405
[ 0.000000] Trying to install interrupt handler for IRQ406
[ 0.000000] Trying to install interrupt handler for IRQ407
[ 0.000000] Trying to install interrupt handler for IRQ408
[ 0.000000] Trying to install type control for IRQ409
[ 0.000000] Trying to set irq flags for IRQ409
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[ 0.000000] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.000000] ... MAX_LOCK_DEPTH: 48
[ 0.000000] ... MAX_LOCKDEP_KEYS: 8191
[ 0.000000] ... CLASSHASH_SIZE: 4096
[ 0.000000] ... MAX_LOCKDEP_ENTRIES: 16384
[ 0.000000] ... MAX_LOCKDEP_CHAINS: 32768
[ 0.000000] ... CHAINHASH_SIZE: 16384
[ 0.000000] memory used by lock dependency info: 3951 kB
[ 0.000000] per task-struct memory footprint: 2304 bytes
[ 0.000000] Calibrating delay loop... 998.84 BogoMIPS (lpj=3899392)
[ 0.000000] pid_max: default: 32768 minimum: 301
[ 0.000000] Security Framework initialized
[ 0.000000] Mount-cache hash table entries: 512
[ 0.000000] CPU: Testing write buffer coherency: ok
[ 0.000000] regulator: core version 0.5
[ 0.000000] regulator: dummy:
[ 0.000000] NET: Registered protocol family 16
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.000000] OMAP DMA hardware revision 5.0
[ 0.052307] bio: create slab <bio-0> at 0
[ 0.055664] regulator: vwl1271: 1800 mV
[ 0.059509] SCSI subsystem initialized
[ 0.068237] usbcore: registered new interface driver usbfs
[ 0.069183] usbcore: registered new interface driver hub
[ 0.069915] usbcore: registered new device driver usb
[ 0.073272] omap_device: omap_i2c.1: new worst case activate latency 0: 30517
[ 0.087310] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz
[ 0.095458] twl4030: PIH (irq 7) chaining IRQs 368..375
[ 0.095611] twl4030: power (irq 373) chaining IRQs 376..383
[ 0.097198] twl4030: gpio (irq 368) chaining IRQs 384..401
[ 0.107330] regulator: VIO: 1800 mV normal standby
[ 0.109283] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby
[ 0.111206] regulator: VDAC: 1800 mV normal standby
[ 0.113159] regulator: VAUX2_4030: 2800 mV normal standby
[ 0.115081] regulator: VPLL2: 1800 mV normal standby
[ 0.116973] regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby
[ 0.118896] regulator: VAUX3: 2800 mV normal standby
[ 0.119995] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.121002] omap_device: omap_i2c.2: new worst case deactivate latency 0: 30517
[ 0.134094] omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
[ 0.140350] Switching to clocksource 32k_counter
[ 0.225463] musb-hdrc: version 6.0, host, debug=0
[ 0.225677] musb-hdrc musb-hdrc.0: degrade from otg to host-only mode
[ 0.225708] musb-hdrc musb-hdrc.0: dma type: dma-inventra
[ 0.225891] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 0.227264] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 0.227874] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.227874] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.227905] usb usb1: Product: MUSB HDRC host driver
[ 0.227905] usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
[ 0.227905] usb usb1: SerialNumber: musb-hdrc.0
[ 0.231384] hub 1-0:1.0: USB hub found
[ 0.231597] hub 1-0:1.0: 1 port detected
[ 0.234649] musb-hdrc musb-hdrc.0: USB Host mode controller at fa0ab000 using DMA, IRQ 92
[ 0.235839] NET: Registered protocol family 2
[ 0.236389] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.237579] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.237854] TCP bind hash table entries: 8192 (order: 6, 360448 bytes)
[ 0.240447] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.240509] TCP reno registered
[ 0.240509] UDP hash table entries: 128 (order: 1, 12288 bytes)
[ 0.240722] UDP-Lite hash table entries: 128 (order: 1, 12288 bytes)
[ 0.241363] NET: Registered protocol family 1
[ 0.242462] RPC: Registered udp transport module.
[ 0.242462] RPC: Registered tcp transport module.
[ 0.242492] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.246063] omap-iommu omap-iommu.0: isp registered
[ 0.246673] AM37x/DM37x Linux PSP version 04.02.00.07 (OMAP3EVM)
[ 0.339263] JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 0.339874] msgmni has been set to 474
[ 0.343963] io scheduler noop registered
[ 0.343994] io scheduler deadline registered
[ 0.344085] io scheduler cfq registered (default)
[ 0.406402] OMAP DSS rev 2.0
[ 0.406799] OMAP DISPC rev 3.0
[ 0.406890] OMAP VENC rev 2
[ 0.407684] OMAP DSI rev 1.0
[ 0.735565] omap_device: omap_i2c.1: new worst case activate latency 0: 61035
[ 0.737426] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.743255] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 1.477935] console [ttyO0] enabled
[ 1.482788] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 1.491180] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 1.499542] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
[ 1.536712] brd: module loaded
[ 1.554290] loop: module loaded
[ 1.561950] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.568786] omap2-nand driver initializing
[ 1.573638] NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix )
[ 1.580535] Creating 5 MTD partitions on "omap2-nand.0":
[ 1.586151] 0x000000000000-0x000000080000 : "X-Loader-NAND"
[ 1.598327] 0x000000080000-0x0000001c0000 : "U-Boot-NAND"
[ 1.608734] 0x0000001c0000-0x000000280000 : "Boot Env-NAND"
[ 1.619110] 0x000000280000-0x000000780000 : "Kernel-NAND"
[ 1.631225] 0x000000780000-0x000020000000 : "File System - NAND"
[ 1.879638] OneNAND driver initializing
[ 1.883972] omap2-onenand omap2-onenand: Cannot request GPMC CS
[ 1.890289] omap2-onenand: probe of omap2-onenand failed with error -16
[ 1.900207] smsc911x: Driver version 2008-10-21.
[ 1.910278] smsc911x-mdio: probed
[ 1.914245] eth0: attached PHY driver [SMSC LAN8700] (mii_bus:phy_addr=ffffffff:01, irq=-1)
[ 1.923339] net eth0: MAC Address: 00:50:c2:7e:98:1c
[ 1.929718] usbcore: registered new interface driver asix
[ 1.935852] usbcore: registered new interface driver cdc_ether
[ 1.942443] usbcore: registered new interface driver net1080
[ 1.948852] usbcore: registered new interface driver cdc_subset
[ 1.955535] usbcore: registered new interface driver zaurus
[ 1.961425] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.968658] omap_device: omap_i2c.1: new worst case activate latency 0: 91552
[ 2.984252] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 2.990295] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2
[ 2.998626] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 3.015625] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 3.021942] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 3.029052] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.036621] usb usb2: Product: OMAP-EHCI Host Controller
[ 3.042205] usb usb2: Manufacturer: Linux 2.6.37 ehci_hcd
[ 3.047851] usb usb2: SerialNumber: ehci-omap.0
[ 3.055145] hub 2-0:1.0: USB hub found
[ 3.059143] hub 2-0:1.0: 3 ports detected
[ 3.094268] Initializing USB Mass Storage driver...
[ 3.099975] usbcore: registered new interface driver usb-storage
[ 3.106292] USB Mass Storage support registered.
[ 3.111694] usbcore: registered new interface driver usbtest
[ 3.117614] udc: OMAP UDC driver, version: 4 October 2004 (iso) (dma)
[ 3.127990] mice: PS/2 mouse device common for all mice
[ 3.136016] input: TWL4030 Keypad as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/twl4030_keypad/0
[ 3.153656] ads7846 spi1.0: touchscreen, irq 335
[ 3.160583] input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input1
[ 3.175292] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrb2
[ 3.189544] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 3.198089] i2c /dev entries driver
[ 3.206451] omap_device: omap_wdt.-1: new worst case activate latency 0: 30517
[ 3.215393] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 3.228637] mmci-omap-hs.1 supply vmmc_aux not found, using dummy regulator
[ 3.311218] usbcore: registered new interface driver usbhid
[ 3.317077] usbhid: USB HID core driver
[ 3.321105] oprofile: hardware counters not available
[ 3.326354] oprofile: using timer interrupt.
[ 3.330993] nf_conntrack version 0.5.0 (3797 buckets, 15188 max)
[ 3.338562] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.344604] TCP cubic registered
[ 3.347961] Initializing XFRM netlink socket
[ 3.352569] NET: Registered protocol family 17
[ 3.357299] NET: Registered protocol family 15
[ 3.362365] Registering the dns_resolver key type
[ 3.367736] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 3.377136] ThumbEE CPU extension supported.
[ 3.393127] Power Management for TI OMAP3.
[ 3.397918] sr_init: No PMIC hook to init smartreflex
[ 3.403594] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 3.412261] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 3.421691] SmartReflex Class3 initialized
[ 3.456573] clock: disabling unused clocks to save power
[ 3.469665] mmc1: card claims to support voltages below the defined range. These will be ignored.
[ 3.496002] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 3.504150] mmc1: new SDIO card at address 0001
[ 3.550201] twl_rtc twl_rtc: setting system clock to 2011-07-07 18:20:40 UTC (1310062840)
[ 6.008361] VFS: Mounted root (jffs2 filesystem) on device 31:4.
[ 6.014739] Freeing init memory: 208K
[ 6.208190] request_module: runaway loop modprobe binfmt-464c
[ 6.214263] request_module: runaway loop modprobe binfmt-464c
[ 6.221191] request_module: runaway loop modprobe binfmt-464c
[ 6.227264] request_module: runaway loop modprobe binfmt-464c
[ 6.235992] request_module: runaway loop modprobe binfmt-464c