Other Parts Discussed in Thread: OMAP3530
HI there
i follow the wiki to use the Codec Engine 2.25's GenServer.pkg to build the H.264 decoder, which got from TI. and it's success to build the h264.x64P.
i modify the server.cfg server.tcf and memmap.tci , replace them with the CE/examples/all_codecs 's files, otherwise , log tell me mem config is not fit with DSPLink config.
then i modify the CE example of Video2_copy, to test if the server is ok, but when dsp run into the Algorithm_create, it's fail..the log is in the file.
plz give me some hint or info to solve this problem, thank you very much!