Part Number: AM623
After the system starts up normally and enters the terminal console, it runs for a period of time and automatically restarts during operation. The chip model is am62x and the SDK version is 10.01.10.04. What is the reason for the restart? Which registers can be read to further troubleshoot the problem?
Read the register 0x431A178h, and there is the following output log:
1 [system reboot time: 1970-01-01 00:00:02] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
2 [system reboot time: 1970-01-01 08:00:01] WARM Reset, Register_value: 0x00010000.
3 [system reboot time: 2026-03-10 01:27:59] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
4 [system reboot time: 2026-03-10 01:34:13] WARM Reset, Register_value: 0x00010000.
5 [system reboot time: 2026-03-10 16:50:43] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
6 [system reboot time: 2026-03-10 18:12:09] WARM Reset, Register_value: 0x00010000.
7 [system reboot time: 2026-03-10 18:19:23] WARM Reset, Register_value: 0x00010000.
8 [system reboot time: 2026-03-10 18:43:16] WARM Reset, Register_value: 0x00010000.
9 [system reboot time: 2026-03-10 22:08:56] WARM Reset, Register_value: 0x00010000.
10 [system reboot time: 2026-03-10 22:12:03] WARM Reset, Register_value: 0x00010000.
11 [system reboot time: 2026-03-10 22:28:24] WARM Reset, Register_value: 0x00010000.
12 [system reboot time: 2026-03-10 22:49:20] WARM Reset, Register_value: 0x00010000.
13 [system reboot time: 2026-03-10 22:55:18] WARM Reset, Register_value: 0x00010000.
14 [system reboot time: 2026-03-10 23:35:19] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
15 [system reboot time: 2026-03-11 00:14:57] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
16 [system reboot time: 2026-03-11 00:54:59] OTHER Reset, Register_value: 0xC0000000.