This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Creating new CSL project for c5515 EZUSB

Hi, I've been trying to create a new project using the CSL files but I seem to run into errors even when trying to create a simple file

Is there anywhere that I can find step by step instructions to be able to create a simple project?

I've been trying to create a new project, where i include all the files that are in the examples

after which i create a main.c and copy the contents of  csl_sar_IntcExample.c

I run into the following errors :

Severity and Description	Path	Resource	Location	Creation Time	Id
errors encountered during linking; "senior_project.out" not built senior_project line 0 1328426897502 257
unresolved symbol _IRQ_clear, first referenced in ./ senior_project line 0 1328426897499 235
unresolved symbol _IRQ_clearAll, first referenced in ./ senior_project line 0 1328426897499 236
unresolved symbol _IRQ_disable, first referenced in ./ senior_project line 0 1328426897500 237
unresolved symbol _IRQ_disableAll, first referenced in ./ senior_project line 0 1328426897500 238
unresolved symbol _IRQ_enable, first referenced in ./ senior_project line 0 1328426897500 239
unresolved symbol _IRQ_globalDisable, first referenced in ./ senior_project line 0 1328426897500 240
unresolved symbol _IRQ_globalEnable, first referenced in ./ senior_project line 0 1328426897500 241
unresolved symbol _IRQ_plug, first referenced in ./ senior_project line 0 1328426897500 242
unresolved symbol _IRQ_setVecs, first referenced in ./ senior_project line 0 1328426897500 243
unresolved symbol _IRQ_test, first referenced in ./ senior_project line 0 1328426897500 244
unresolved symbol _SAR_A2DMeasParamSet, first referenced in ./ senior_project line 0 1328426897501 245
unresolved symbol _SAR_chanClose, first referenced in ./ senior_project line 0 1328426897501 246
unresolved symbol _SAR_chanCycSet, first referenced in ./ senior_project line 0 1328426897501 247
unresolved symbol _SAR_chanInit, first referenced in ./ senior_project line 0 1328426897501 248
unresolved symbol _SAR_chanOpen, first referenced in ./ senior_project line 0 1328426897501 249
unresolved symbol _SAR_chanSetup, first referenced in ./ senior_project line 0 1328426897501 250
unresolved symbol _SAR_deInit, first referenced in ./ senior_project line 0 1328426897501 251
unresolved symbol _SAR_init, first referenced in ./ senior_project line 0 1328426897501 252
unresolved symbol _SAR_readData, first referenced in ./ senior_project line 0 1328426897502 253
unresolved symbol _SAR_startConversion, first referenced in ./ senior_project line 0 1328426897502 254
unresolved symbol _SAR_stopConversion, first referenced in ./ senior_project line 0 1328426897502 255
unresolved symbol _VECSTART, first referenced in ./ senior_project line 0 1328426897502 256

After switching to algebraic assembly source langauge build (which i see some people recommend), i get: 

Severity and Description	Path	Resource	Location	Creation Time	Id
[E0000] parse error senior_project line 0 1328426083055 233
[E0003] Only labels and comments may begin in the first column. Make sure that the label name is not a reserved keyword. senior_project line 0 1328426083056 234
[E0004] Substitution symbol operand expected senior_project line 0 1328426083055 232