This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing external memory with dsk6713

I want to increase the memory available on the DSK 6713 board.

I want to interface an external memory to the EMIF.

Now i am not sure what memories are supported by the DSK6713.

I am also confused between selecting and SBSRAM or SDRAM

I want to know the name of the supported Memories

that can be interfaced with DSK6713 using EMIF.

I have heard about the Micron's SBSRAM "MT58L512Y32P".

This is supported by c55x.Not sure about the DSK6713.

Please help.

Thanks,

Mehul Saxena