Part Number: TDA4VL-Q1
Other Parts Discussed in Thread: TDA4VL
What are the recommended POK TRIM value settings for each POK instance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
THE POK Threshold TRIM refers to Software-configurable values (0-127) to set UV/OV detection thresholds. This is a 7 bit value (0-127) configured via the POK control registers for each instance. The POK trim values have different valid ranges depending on the POK type. Not all values 0-127 are valid.
The TDA4VL device TRM has below "POK Threshold Levels" table for the limits -

In summary, the following table shows the ranges for each POK type based on TI validation -
| UV Threshold (in hex) | OV Threshold (in hex) | |
| Core | 0x0 - 0x46 | 0x0 - 0x4A |
| 1.8V | 0x20 - 0x44 | 0xC - 0x30 |
| 3.3V | 0x0 - 0x44 | 0x0 - 0x2F |
Note: The above ranges are inclusive. Values outside these ranges produce undefined/invalid behavior.
To calculate the TRIM values based on your target voltage, the following approach is recommended -
Regards,
Josiitaa