This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem running a sys/bios hello example within the ccs5 simulator...

Other Parts Discussed in Thread: SYSBIOS

Hello !

I'm trying to run a sys/bios example application with the ccs 5.1.0.09 simulator doing the following:

creating a new ccs project, choosing sys/bios examples hello with c6000 family device and a "Generic c674x device" variant,

next I'm choosing a dm8148 platform (which is my target platform eventually)

The application builds fine.

Then I'm creating a target configuration file, choosing c674x CPU Cycle accurate simulator, little endian.

I'm placing a breakpoint on the first line of the main function and run the simulator.

The simulator seems to run but the breakpoint never triggered, if I suspends the cpu it looks like the device

runs the clock ticker, I see in the stack that starting from address 0

then deviceConfig from Timer.c

then ti_sysbios_knl_doTick... from hello_p674.c:2,567

then ti_sysbios_timers... from Timer.c:553

then deviceConfig... from Timer.c:186

did I miss something ?