I got strange relationship of ISS clock and video data frame rate in DM8148.
My configuration is connect camera sensor OV10630 with discrete sync in VIN1 PortA of HDVPSS.
The VIN format is BT.656 8bit.
When I set ISS clock as 400Mhz, the video frame rate is about 14fps.
But, when I reduce ISS clock to 200Mhz, the video frame rate raise to about 28fps.
According to data sheet, the clock source of ISS and Media Controller (VPSS-M3 and Video-M3) is PLL_MEDIACTL.
When I increase ISS clock to 400Mhz, the M3 clock should also become 400Mhz, it should increase M3 processing frequency and the video frame rate should become higher theoretically.
Does anyone can help to explain this testing result???
Best regards,
Albert Ke