This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VL-Q1: ECC Self Test Procedure

Part Number: TDA4VL-Q1

What is the effort required by the system integrator to enable and test ECC on the different IPs on the SoC using ECC aggregators? 

  • Hi, 

    Please refer to the table below for details on how each ECC endpoint can be tested using ECC aggregators - 

    ECC Type Inject Type Accessible Mem Checker Type Single bit injection possible? Test Procedure Double bits injection possible? Test Procedure
    ECC Wrapper
    Inject only NO N/A Yes SDL APIs can be used only for error injection. Error detection and correction is a part of the IP itself. Yes SDL APIs can be used only for error injection by forcefully setting the error status bits. Error detection and correction is a part of the IP itself.
    Inject with error capture YES N/A Yes SDL APIs can be used, memory access also a part of the SDL ecc_func_app in sdl/test Yes SDL APIs can be used, memory access also a part of the SDL ecc_func_app in sdl/test
    Inject with error capture NO N/A Yes

    SDL APIs can be used only to inject error

    Details on memory access to trigger error available in - [FAQ] TDA4VL-Q1: ECC Testing Procedure for Inaccessible RAM IDs and [FAQ] TDA4VH-Q1: ECC Testing Procedure for Inaccessible RAM IDs

    No

    SDL APIs can be used only to inject error by forcefully setting the error status bits. No requirement to perform a memory access.

    EDC Interconnect
    Inject with error capture
    NO
    Redundant Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test No N/A
    Parity Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test No N/A
    Error Detect and Correct Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test
    YES Redundant Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test No N/A
    Parity Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test No N/A
    Error Detect and Correct Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test Yes SDL APIs can be used, no memory access required. Refer ecc_func_app in sdl/test

    For details on the meaning and types of ECC endpoints, please refer - [FAQ] TDA4VM: Types of ECC Aggregators, RAM IDs and Error Injection

    Regards,

    Josiitaa