This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 Silicon Rev 2.0 Clocking Capabilities

Other Parts Discussed in Thread: OMAP-L138

We are currently using an OMAP-L138 commercial grade part and an OMAP-L138 industrial grade part. We are buying the SOM modules from LogicPD and I am wondering if the processors that we have can both run at the maximum 456Mhz clock speed given a core voltage of 1.3V.  Here are the OMAP-L138 part labels:

 OMAPL138BZCE  08ALFLW GI  A375  (commercial grade part on the LogicPD SOMOMAPL138-10-1502QHCR-A)

OMAPL138BZCE  0AA2GSW GI  A375 (industrial grade part on the Logic PD SOMOMAPL138-10-1602QHIR-A)

 Based on the L138 data sheet we are using silicon rev 2.0 parts.  I believe that the L138 data sheet shows we should be able to run both parts up to 456MHz if we provide a core voltage of 1.3V.  Is this correct?