Other Parts Discussed in Thread: AM1808
Hi,
We are using the AM1808-SOM-M1 module on a custom baseboard that we made, which is similar to the evaluation module. We want to boot from the SPI flash, which is the default boot mode of the module. However, it appears that when the module is connected to our baseboard, something prevents the boot to complete correctly. It freezes when it seems to try to run from the DDR2, but since everything is embedded on the module, we don't know what could be the cause of this issue.
Here's a log from the uart console:
AM1808 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: SPI
Starting SPI Memory Copy...
Valid magicnum, 0x55424CBB, found at offset 0x00010000.
DONE
Jumping to entry point at 0xC1080000.
ú[00]
When we use the same module on the evaluation board, it boots correctly!!?!
Any ideas?
Regards,
Yannick