Hello,
This may seem like a stupid question, but I am asking it anyway. The datasheet says that the power-down sequence should be the exact reverse of the power-up sequence. I have seen the other forum posts on this topic, including one in which my same questions was asked, but not explicitly answered.
My question is this: Do the clocks and other resets need to be included as part of the power down sequence, or are the power rails alone sufficient? In other words, can I disable the clocks and assert the resets as soon as POR or RESETFULL is asserted, then sequence through turning off each power rail. Or should I sequence the resets and clocks as well?
Thank you very much.
-Courtney