Other Parts Discussed in Thread: OMAP3530
hi all
i am working on OMAP3530 and 256 MB NAND flash used for booting.
my question is,
how to use some portion of NAND flash as a mass storage device?
i have done some changes in /arch/arm/mach-omap2/board_omap3devkit8000.c to create extra mtd partition.
actual NAND flash partitions are
0x00000000-0x00080000 : "X-Loader"
0x00080000-0x00260000 : "U-Boot"
0x00260000-0x00280000 : "U-Boot Env"
0x00280000-0x00680000 : "Kernel"
0x00680000-0x10000000 : "File System"
After creating one more extra partition called EXTENDED PARTITION
0x00000000-0x00080000 : "X-Loader"
0x00080000-0x00260000 : "U-Boot"
0x00260000-0x00280000 : "U-Boot Env"
0x00280000-0x00680000 : "Kernel"
0x00680000-0x01940000 : "File System"
0x01940000-0x10000000 : "EXTENDED PARTITION"
i created uImage and working fine if booting from SD Card.
but not booting from NAND flash
i have attached the console output file, please refer and suggest me..
thanks and Regards
N Reddy