Part Number: AM62A7
Greetings,
I have a query about the DRP (Dual-Role Port) configuration on the AM62A EVM. How can I set up the board to act as a peripheral when connected to a laptop via USB?
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62A7
Greetings,
I have a query about the DRP (Dual-Role Port) configuration on the AM62A EVM. How can I set up the board to act as a peripheral when connected to a laptop via USB?
Regards.
Hi,
I am routing this thread to our expert for further comments. Please except reply in a day or two.
You can follow the instruction provided at USB Device to configure USB in device mode.
Regards,
Tushar
Hi Wilberth,
The USB port mode is configured in the devicetree. The SDK Linux already configures the USB0 port (to the USB type-C connector on SK-AM62A EVM) to be the dual role port. The only thing you need to do is load a USB gadget driver of your choice after the Linux is booted on the EVM.