This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x-PSP

Hi,

I have questions regarding AM335x PSP 04.06.0.00.03 version.

Our customer is using the above version of PSP.

According to the release note, the following issues are written in it as known issues.

1)SDOCM0008576[30] : USB: devices connected through a full speed(USB1.1)hub fail to wrok in DMA mode.

2) SDOCM00087342[60] : USB : CPPI4.1 DMA locks up when CPU mode transfer is done in parallel to DMA transfer.

On customer's application, the above both cases may be happened.

So customer would like to know that these issues are caused by hardware issue of device or software issue of the kernel.

Of course, it is preferable the cause is sofware issue. If it is software issue, when is it fixed?

Please advise me.

Best regards,

Michi