This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting cmos sensor directly to DM6437 problem

I still confuse in the DVSDK preview on the fly FVID_exchange problem.

I wonder whether it's valid to connect a cmos sensor "directly" to the DC_P1 & DC_P2  on the dm6437 board.

It means there's no image card between the image sensor and dm6437 board!!!

Databus D[7:0] ,HD ,VD ,i2c_clk ,i2c_data are connected to DC_P1 & DC_P2 externally .

Most people use their camera which already has composite video connector connecting to the video port on dm6437.

Is there anyone done this before ?