Part Number: AM3358
Hi
We designed a custom board using AM3358ZCZ PCB, We are facing an issue to load SPL uboot and uboot using usb_ether.
Below is the Log: After ", eth1: usb_ether" usb Detection fails in Linux, it is no more detect as RNDIS, enumeration fails and system hung. This happens in only 2025.01 uboot. At sametime we have working uboot with 2020 uboot, all works good.
U-Boot SPL 2025.01-00006-g07019a6c6097-dirty (Mar 27 2026 - 19:14:02 +0530)
Trying to boot from USB eth
File: drivers/net/ti/cpsw.c, Function: cpsw_eth_probe, Line: 1090
eth0: eth_cpsw
AM I CORRECT
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC de:ad:be:ef:00:01
HOST MAC de:ad:be:ef:00:00
RNDIS ready
, eth1: usb_ether
Any clue how to fix this issue with 2025 uboot. This can be easily reproducable in beagleboneblack and AM335x-EVM. We can able to reproduce with Beaglebone black. Issue with only 2025.01 Uboot. Release.
Rgds
Chandra