Other Parts Discussed in Thread: TMS320C5505
All:
I am working on an "already defined" project based on DSP-BIOS 5.41.11.38 and the TMS320C5505 processor. I would like to see an enhancement to DSP-BIOS to show in a report what has changed from the default DSP-BIOS .TCF setup.
Right now, I need to "comb thru" the GUI, and it is easy to see when tasks or SWIs are added. What is not as easily detected are things like HWI changes or memory changes.
Having such a tool would benefit someone coming into a program at a point other than the beginning, and it would also help in documenting what has gone on with a project.
Regards,
Todd Anderson