Part Number: SK-AM62P-LP
Other Parts Discussed in Thread: AM62P, LM5141, AM623
Hi Experts,
We are using the AM62P SK EVM for an DMS camera application. The board was functioning normally and running a camera pipeline demo. During runtime, the board suddenly powered off and is no longer booting.
Board revision: PROC164E2
Current observations:
- USB-C(PWR) input voltage is present (12.09V via PD negotiation) (TP204)
- Input voltage present at VMAIN( TP82) = 12.09V
- Only one LED glowing. (USB PWR LED)
- No output voltage observed on inductors (L1/L2/L4) in the LM5141 power stage
- No voltage across bulk capacitors (near KEMET capacitors)
- No heating observed on power components
- Board shows no boot activity (no rails, no UART output)
Please help us with this.
Thanks and regards.
Eliza