This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: OSPI Flash Programming Using External TI Debugger/Download Cable XDS110

Part Number: TMDS64EVM

Hello,

Is it possible to flash an image to OSPI flash on TMDS64EVM development board using the external debugger/download cable XDS110 using WIndow command lines and NOT using the Code Composer Studio tool ?

I need to find this as the faster programming  alternative instead of using UART Boot and download.

It is for production programming step in which no CCS is installed.

Is it possible ? If it is then what needs to bedone.

Thank you.

H. Nguyen