Part Number: J784S4XEVM
Other Parts Discussed in Thread: USB2ANY
Hello,
I am experiencing a fault where the EVM shuts off semi-randomly after a while and it works just fine until it happens. What I also noticed is that the MCUIO_3V3 and VSYS_IO_3V3 LEDs flicker a few times just before shutoff.
The shutoff happens after ~15-45 minutes after a cold bootup (after sufficient "cool-off" time), but happens either immediately (a few seconds) or in a few minutes if I cycle power after it shuts off once.
This all sounds like something is overheating but I didn't spot anything unusually hot with a thermal camera. What we also tried is to replace the SD card from a working board to rule out anything software related and cross checked that the switch positions are the same.
Here is a video of the LED behavior (reduced to last 10 seconds, and you can also see the fan spinning down);
I can re-upload the video in slow-mo if the flicker behavior isn't obvious but they flicker very quickly and turn off.
What do you suggest for diving deeper on the issue? I do have an oscilloscope and I can probe the board if it helps.