I have the ezDSP5535. How can I obtain the Pure Path Audio tool for the aic3204 and a possible upgrade to the aic3254?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have the ezDSP5535. How can I obtain the Pure Path Audio tool for the aic3204 and a possible upgrade to the aic3254?
Hi,
You can get it from http://www.ti.com/tool/aicpurepath_studio.
I want to make sure that ezDSP5535 is not aic3204 EVM. So Pure Path Audio tool cannot be used with ezDSP5535 board. However you can use Pure Audio tool without EVM.
Regards,
Hyun
I checked the Audio Converter group forum and found this path for Pure Path Studio request:
http://www.ti.com/tool/aicpurepath_studio
Regards.
Hyun,
I requested the purepath studio last night. Any idea how long it takes them to approve? And if not approved would they notify me anyway?
It's OK if it doesn't work with the ezDSP5535, it will help me figure out if I can use the mini DSP in the overall system I'm working on. One side may have the 5535, the other the mini DSP. Also am considering using mini DSP with the cc5535 to do some pre processing. Seems only way to know what's possible with mini DSP is to get pure path studio.
Thanks,