This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

custom applications on omap l138! linux not booting

hello everyone!

i am beginner with omap l138. i am booting linux from sd card which i prepared using instructions given in "software development guide" , Also i tested few sample applications using CCS5.1 in the debug mode, however when i try to flash the image in the SPI, the program works but the linux fails to boot. i created the .bin( generated using AISgen) and used the serial flasher to flash both the application image file and "arm-mmcd.bin" for u-boot. when i restart the board, the application runs but the linux doesnt boot.

my application just scrolls a message in the character LCD. Can anybody suggest what is the possible issue? am i missing something?

thanks

regards

hitesh